Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DisplayInDrawings | Controls whether or not the referenced part or assembly is visible in the draft environment. |
DisplayInSubAssembly | Specifies whether the referenced Part is shown or hidden when this assembly is inserted into another assembly. |
FaceStyle | Sets and returns the FaceStyle object for the referenced Occurrence. |
IncludeInBom | Controls whether or not the referenced part is included in reports. |
IncludeInPhysicalProperties | Controls whether or not the referenced Part is included in physical property calculations. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
IsForeign | Specifies whether or not the referenced Part orginated from an application other than Solid Edge. |
Locatable | Sets and returns the referenced object's locatable state. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
PartDocument | Returns the PartDocument object for the active Part. |
PartFileName | Returns the name of the data file for the PartDocument object of the active part. |
Quantity | Returns the number of occurrences of the referenced object. |
ReferenceOnly | Returns the 'reference-only' state of the active Part. |
Relations3d | Returns a collection of Relations3d objects for the referenced Part. |
Status | Returns the status (a member of the PartStatusConstants constant set) of the referenced Part. |
Style | Returns the style for the referenced object. |
Subassembly | Returns True if the referenced object is a subassembly. |
Type | A member of the ObjectType constant set. |
Visible | Controls the display of the referenced object. |