Solid Edge Assembly Type Library
EndpointMagnitude Property
Collapse All
Expand All
Solid Edge Assembly Type Library
>
Path Object
: EndpointMagnitude Property
Description
Sets and returns the direction and degree of influence of the EndpointEdge on the curvature of the curve at the endpoint.
Property type
Read-only property
Syntax
Visual Basic
Public Property EndpointMagnitude As Double
Remarks
This value is meaningful only if the EndpointEndCondition is seKeypointEndConditionTangent.
See Also
Path Object
|
Path Members
|
Solid Edge V18 - What's New