Solid Edge Assembly Type Library
WriteToFile Method
Specifies the name of the text file to be created.
Description
Creates a text file that contains the physical property information for the referenced assembly.
Syntax
Visual Basic
Public Sub WriteToFile( _
   ByVal FileName As String _
) 
Parameters
FileName
Specifies the name of the text file to be created.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objPhyProps As SolidEdgeAssembly.PhysicalProperties
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
    Dim Filedt As Variant
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Close the active document
    Call objDoc.Close
    ' opening an existing assembly file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Getting the PhysicalProperties object of the assembly document
    Set objPhyProps = objDoc.PhysicalProperties
    ' Compute the physical properties.
    Call objPhyProps.Update
    ' Write the physicalproperties information in to a file.
    Call objPhyProps.WriteToFile(Filename:="T:/temp/PhysicalProp")
    ' Getting date and time of a created file
    Filedt = FileDateTime("T:/temp/PhysicalProp")

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPhyProps = Nothing
End Sub
See Also

PhysicalProperties Object  | PhysicalProperties Members