Solid Edge Assembly Type Library
Count Property
Description
Returns the number of objects in the referenced collection.
Property type
Read-only property
Syntax
Visual Basic
Public Property Count As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objPart As SolidEdgeAssembly.Occurrence
    Dim objRelations3d As SolidEdgeAssembly.Relations3d
    Dim lngCount As Long
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening an existing assembly document
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting a particular part from the assembly
    Set objPart = objDoc.Occurrences.Item(2)
    ' getting the relations3d object for the part
    Set objRelations3d = objPart.Relations3d
    ' getting the count of relations in the Relations3d collection object
    lngCount = objRelations3d.Count
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPart = Nothing
    Set objRelations3d = Nothing
End Sub
See Also

Relations3d Collection  | Relations3d Members