Solid Edge Assembly Type Library : SubOccurrence Object |
CreateTopologyReference | Creates a TopologyReference object that points to a topological (G&T) element contained within the definition of the referenced Occurrence or SubOccurrence object. |
CreateTopologyReferenceToBodyOverride | |
FileMissing | Returns a bool value stating the file is missing or not |
GetAdjustablePart | Returns the adjustable part object. |
GetBodyInversionMatrix | |
GetExplodeMatrix | |
GetInterpartDrivenOccurrences | |
GetInterpartDrivingOccurrences | |
GetMaterial | Returns the material conditions for the referenced SubOccurrence object. |
GetMatrix | Returns the transformation matrix for the referenced suboccurrence. |
GetReferenceKey | Returns a reference key for the referenced object. |
GetSimplifiedBodies | |
MakeAdjustablePart | This method makes the part in the referenced Occurrence object an adjustable part. |
PutMatrix | Sets the transformation matrix for the referenced occurrence. |
Range | |
RecheckMissingFile | Returns a bool value if the file is found which was previously missing |
RemoveOverrideBody | This method removes the dumb override body that exists on the assembly occurrence. |
Adjustable | Specifies whether the referenced object is adjustable. |
Application | Returns the active application object. |
Body | Returns the Body object for the referenced object. |
CoordinateSystemsVisible | |
DisplayAsLastSaved | Specifies whether the last saved display is visible in the referenced object. |
DisplayCenterline | |
DisplayConstrCurves | Specifies whether construction curves are visible in the referenced object. |
DisplayConstructions | Specifies whether constructions are visible in the referenced object. |
DisplayCoordinateSystems | Specifies whether coordinate systems are visible in the referenced object. |
DisplayReferenceAxes | Specifies whether reference axes are visible in the referenced object. |
DisplayReferencePlanes | Specifies whether reference planes are visible in the referenced object. |
DisplaySketches | Specifies whether sketches are visible in the referenced object. |
HasBodyOverride | Creation of an assembly feature, for example, on an SubOccurrence of an assembly results in an override body being created for the SubOccurrence in the context of the assembly. Solid Edge uses the override body in place of the body from the SubOccurrence document in the assembly for display, interference analysis etc. |
IsAdjustablePart | Tests whether part is adjustable part. |
IsPatterned | |
IsPatternItem | |
ItemNumber | |
Name | Returns the name of the referenced object. |
NodeType | |
Parent | Returns the parent object for the referenced object. |
Reference | |
ReferencePlanesVisible | |
SketchesVisible | |
Subassembly | Returns True if the referenced object is a subassembly. |
SubassemblyBodies | |
SubOccurrenceDocument | Returns the suboccurrence document object. |
SubOccurrenceFileName | Returns the suboccurrence file name. |
SubOccurrences | Returns the SubOccurrences collection object that enumerates the next level sub-occurrence objects. |
ThisAsOccurrence | This read-only property returns the Occurrence object to which the referenced SubOccurrence object belongs. |
TopLevelDocument | Returns the toplevel AssemblyDocument object. |
Type | A member of the ObjectType constant set. |
UseSimplified | Returns True if the referenced object is using a simplified model. |
Visible | Controls the display of the sub-occurrence |