Solid Edge Assembly Type Library : SubassemblyBody Object |
GetMaterial | This method returns the material conditions for the referenced object. |
GetReferenceKey | Returns a reference key for the referenced object. |
Application | Returns the active application object. |
AssemblyBodyType | |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Body | Returns the Body object for the referenced object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Reference | |
ThisAsAssemblyBody | |
TopLevelDocument | Returns the toplevel AssemblyDocument object. |
Type | A member of the ObjectType constant set. |
Visible | Controls the display of the referenced object. |