Solid Edge Assembly Type Library : Zone Object |
AddPartsToSelectSet | This method adds all of the parts to the select set that satisfy the zone definition. |
CopyToClipboard | Copies the referenced object to the operating system clipboard. |
GetPoints | This method returns six points that define the low and high corners of the box. |
Hide | This method hides the referenced object. |
HideParts | This method hides all parts that satisfy the zone definition. |
IsVisible | This method returns True if the referenced object is visible and False if not. |
PopulateFromClipboard | Populates the zone from the operating system clipboard. |
SetPoints | This method sets six points that define the low and high corners of the box. |
Show | |
ShowOnlyParts | This method shows only the parts that satisfy the zone definition. All other parts are hidden. |
ShowParts | This method shows all of the parts that satisfy the zone definition. |
Application | |
Name | Returns the name of the referenced object. |
Overlap | This read-write property sets or returns the overlap for the zone. |
Parent |