ActiveSection | Returns the active sheet's Section object. Sheets are grouped into sections: WorkingSection, BackgroundSection, and 2dModelSection. |
ActiveSectionType | Specifies the type of Section that the active sheet is a member of. |
ActiveSheet | Returns the active Sheet object. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Backdrop | Returns the BackDrop object for the referenced SheetWindow object. |
Caption | Sets and returns the caption of the referenced object. |
Display2DModelSheetTab | |
DisplayAsPrinted | Specifies whether or not the objects that belong to the referenced SheetWindow object are displayed as they will print. |
DisplayBackgroundSheetTabs | |
DisplayHScroll | Specifies whether or not the horizontal scroll bar is displayed. |
DisplaySheetTabs | Specifies whether or not sheet tabs for the referenced SheetWindow object are displayed. |
DisplayVScroll | Specifies whether or not the vertical scroll bar is displayed. |
DisplayWorkingSheetTabs | |
Environment | Returns the Environment object for the referenced Window object. |
Height | Returns the height of the referenced object. |
hWnd | Returns the window handle for the referenced object. |
Icon | Returns the collapse icon handle (HICON) for the referenced Window object. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Left | Specifies the distance (in twips) between the internal left edge of an object and the left edge of its container. |
Parent | Returns the parent object for the referenced object. |
SelectedSheets | Returns a collection of all selected sheets in the referenced window. |
SelectSet | Returns the current selection set for the referenced document. |
SheetTabRatio | Sets and returns the ratio of the width of the window sheet tabs to the width of the window horizontal scrollbar. |
Top | Sets and returns the distance from the top edge of the physical screen to the top edge of the main application window. |
TransparentDisplay | Specifies whether or not transparent display is on. |
Type | Specifies the type of the object being referenced. |
UsableHeight | Returns the height of the usable vertical space in the application window area. |
UsableWidth | Returns the height of the usable vertical space in the application window area. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |
Width | Returns the width of the referenced object. |
WindowNumber | Returns the window number of the referenced Window object. |
WindowState | Sets and returns the state of the referenced window. |
Zoom | Sets and returns the display size of the window contents. |