Solid Edge Draft Type Library
Top Property
Collapse All
Expand All
Solid Edge Draft Type Library
>
SheetWindow Object
: Top Property
Description
Sets and returns the distance from the top edge of the physical screen to the top edge of the main application window.
Property type
Read-write property
Syntax
Visual Basic
Public Property Top As Integer
Remarks
Sets and returns the distance from the top edge of the physical screen to the top edge of the main application window, in points (1/72 inch).
See Also
SheetWindow Object
|
SheetWindow Members