Solid Edge Draft Type Library
UsableWidth Property
Collapse All
Expand All
Solid Edge Draft Type Library
>
SheetWindow Object
: UsableWidth Property
Description
Returns the height of the usable vertical space in the application window area.
Property type
Read-only property
Syntax
Visual Basic
Public Property UsableWidth As Integer
Remarks
The width is returned in points (1/72 inch). Adding section tabs or a vertical scroll bar reduces the usable width.
See Also
SheetWindow Object
|
SheetWindow Members