Solid Edge Draft Type Library
Zoom Property
Collapse All
Expand All
Solid Edge Draft Type Library
>
SheetWindow Object
: Zoom Property
Description
Sets and returns the display size of the window contents.
Property type
Read-write property
Syntax
Visual Basic
Public Property Zoom As Double
Remarks
A setting of 100 means that the window contents are shown at their normal size; 50 means that the window contents are shown at half size.
See Also
SheetWindow Object
|
SheetWindow Members