Solid Edge FrameworkSupport Type Library : AreaProperties Object |
AddBoundaries | This method creates a blend between edges, faces, or a combination of the two. |
BringForward | |
BringToFront | |
Copy | |
Cut | |
Delete | Deletes the referenced object. |
Duplicate | |
GetAreaProperties | |
Mirror | Copies the referenced object about an axis. |
Move | Moves the referenced object. |
Range | Returns the high and low range values for the referenced object. |
Rotate | Rotates the referenced object. |
Scale | Scales the referenced object by a specified factor. |
SendBackward | This method changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it. |
SendToBack | This method changes the display order of visible objects by moving the referenced object behind all overlapping objects. |
SetAxesLabels | |
SetAxesLength | |
ShowAxes |
Application | |
AreaFillStyle | Returns the Shells collection object for the referenced Body object. |
AxesLabelStyle | |
AxesStyle | |
Document | Returns the document to which the referenced object belongs. |
Index | Returns the numeric index for the active object. |
Key | |
Layer | Sets and returns the named layer on which the referenced object resides. |
Name | Returns the name of the referenced object. |
Parent | |
Type | Specifies the type of the object being referenced. |