Solid Edge FrameworkSupport Type Library : Boundary2d Object |
BringForward | Changes the display order of the referenced object by moving it in front of the first object that obscures it. |
BringToFront | Changes the display order of the referenced object by moving it in front of all other overlapping objects. |
ConstructGeometry | Constructs geometric objects on the perimeter of the region of the referenced Boundary2d object. |
Copy | Places a copy of the referenced object on the clipboard. |
Cut | Moves the referenced object to the system clipboard. |
Delete | Deletes the referenced object. |
Duplicate | Copies the referenced object to a specified location, creating a new instance of the object with the same property values as the original. |
GetCentroid | Returns the coordinates of the centroid of the referenced object. |
GetFloodPoint | Returns the coordinates of the boundary flood point. |
GetKeyPoint | Returns information about a specified key point. |
Mirror | Copies the referenced object about an axis. |
Move | Moves the referenced object. |
Range | Returns the high and low range values for the referenced object. |
Rotate | Rotates the referenced object about the point specified by the angle in radians. |
Scale | Scales the referenced object by a specified factor. |
Select | Selects the referenced object in the active window. |
SendBackward | Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it. |
SendToBack | Changes the display order of visible objects by moving the referenced object behind all overlapping objects. |
SetKeyPoint | Sets the position for a specified key point. |
Application | Returns the active application object. |
Area | Returns the area of the referenced object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BoundingObjects | Returns the BoundingObjects2d collection object for the referenced Boundary2d object. |
Document | Returns the document to which the referenced object belongs. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. |
Layer | Sets and returns the named layer on which the referenced object resides. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Perimeter | Returns the total length along the border of the referenced object. |
State | Returns the current state of the referenced boundary. |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
Type | Specifies the type of the object being referenced. |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |