Solid Edge FrameworkSupport Type Library
BringForward Method
Description
Changes the display order of the referenced object by moving it in front of the first object that obscures it.
Syntax
Visual Basic
Public Sub BringForward() 
Remarks
This command is useful when other objects that are filled hide an object and the user wants to remove the object from hiding while not bringing the object to the top of the priority list.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objBounds As SolidEdgeFrameworkSupport.Boundaries2d
    Dim objBound(2) As SolidEdgeFrameworkSupport.Boundary2d
    Dim dblPoint(1 To 8) As Double
    Dim i As Integer
    Dim j As Integer
    Dim lngOrder As Long
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Get the Boundaries2d object on the active sheet
    Set objBounds = objSheet.Boundaries2d
    ' Create a Points array
    dblPoint(1) = 0.1
    dblPoint(2) = 0.1
    dblPoint(3) = 0.1
    dblPoint(4) = 0.2
    dblPoint(5) = 0.2
    dblPoint(6) = 0.2
    dblPoint(7) = 0.2
    dblPoint(8) = 0.1
    ' Create a Boundary2d objects
    For j = 0 To 2
        Set objBound(j) = objBounds.AddByPoints(PointCount:=4, Points:=dblPoint)
        ' Change points in the array
        For i = 1 To 8
            dblPoint(i) = (dblPoint(i) + 0.05)
        Next i
    Next j
    'Get current Zorder
    lngOrder = objBound(0).ZOrder
    'BringForward the object
    Call objBound(0).BringForward

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objBounds = Nothing
    Set objBound(0) = Nothing
    Set objBound(1) = Nothing
    Set objBound(2) = Nothing
End Sub
See Also

Boundary2d Object  | Boundary2d Members