Solid Edge FrameworkSupport Type Library
GetCentroid Method
The coordinates of the centroid for the referenced object.
The coordinates of the centroid for the referenced object.
Description
Returns the coordinates of the centroid of the referenced object.
Syntax
Visual Basic
Public Sub GetCentroid( _
   ByRef x As Double, _
   ByRef y As Double _
) 
Parameters
x
The coordinates of the centroid for the referenced object.
y
The coordinates of the centroid for the referenced object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objBounds As SolidEdgeFrameworkSupport.Boundaries2d
    Dim objBound As SolidEdgeFrameworkSupport.Boundary2d
    Dim dblPoint(1 To 8) As Double
    Dim dblX As Double, dblY As Double
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Get the Boundaries2d object on the active sheet
    Set objBounds = objSheet.Boundaries2d
    ' Create a Points array
    dblPoint(1) = 0.1
    dblPoint(2) = 0.1
    dblPoint(3) = 0.1
    dblPoint(4) = 0.2
    dblPoint(5) = 0.2
    dblPoint(6) = 0.2
    dblPoint(7) = 0.2
    dblPoint(8) = 0.1
    ' Create a Boundary2d object
    Set objBound = objBounds.AddByPoints(PointCount:=4, Points:=dblPoint)
    'Get Centroid of the boundary
    Call objBound.GetCentroid(x:=dblX, y:=dblY)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objBounds = Nothing
    Set objBound = Nothing
End Sub
See Also

Boundary2d Object  | Boundary2d Members