Solid Edge FrameworkSupport Type Library > Boundary2d Object : GetFloodPoint Method |
The flood point is the point given to the AddByObjects method which is used to select the region to be filled. When a Boundary2d object is selected, a handle is displayed at the flood point. The flood point is always contained within the region defined by the Boundary2d object.
GetFloodPoint is not supported for boundaries from section views. Boundaries created by the Section View process don't have flood points or keypoints because they are created by internal procedures to Solid Edge.
Since they are generated by the system, we can’t return points that we don’t have. We consistently return a position of x=1.0e+30 and y=1.0e+30, which is used internally to indicate an invalid or infinite coordinate. The programmer can reliably check for these numbers to determine that the floodpoint or handlepoint is undefined.
Private Sub Form_Load() Dim objApp As SolidEdgeFramework.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objBounds As SolidEdgeFrameworkSupport.Boundaries2d Dim objBound As SolidEdgeFrameworkSupport.Boundary2d Dim dblPoint(1 To 8) As Double Dim dblX As Double, dblY As Double ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If 'Get the Active Sheet object Set objSheet = objDoc.ActiveSheet 'Get the Boundaries2d object on the active sheet Set objBounds = objSheet.Boundaries2d ' Create a Points array dblPoint(1) = 0.1 dblPoint(2) = 0.1 dblPoint(3) = 0.1 dblPoint(4) = 0.2 dblPoint(5) = 0.2 dblPoint(6) = 0.2 dblPoint(7) = 0.2 dblPoint(8) = 0.1 ' Create a Boundary2d object Set objBound = objBounds.AddByPoints(PointCount:=4, Points:=dblPoint) 'Get FloodPoint of the boundary Call objBound.GetFloodPoint(x:=dblX, y:=dblY) ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objSheet = Nothing Set objBounds = Nothing Set objBound = Nothing End Sub