Solid Edge FrameworkSupport Type Library
ComplexString2d Object
Members 
Description
A string of endpoint-coincident 2-D geometry objects.
Object Model
ComplexString2d ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionDrawingObjects CollectionGeometryStyle2d Object
Remarks
he ComplexString2d object acts as an owner of the objects that comprise the complex string. Thus, the complex string is manipulated as a single object. A ComplexString2d object can be closed or open depending on whether the first object's start point is coincident with the last object's endpoint. All objects that constitute the complex string have the same display style. The ComplexString2d object is not available to the interactive user. It is exposed to automation to provide an additional tool to the programmer for creating more complex commands.
See Also

ComplexString2d Members