BringForward | Changes the display order of the referenced object by moving it in front of the first object that obscures it. |
BringToFront | Changes the display order of the referenced object by moving it in front of all other overlapping objects. |
Copy | Places a copy of the referenced object on the clipboard. |
Cut | Moves the referenced object to the system clipboard. |
Delete | Deletes the referenced object. |
GetCenterElement | This function returns the center element, center point and the key point index. If the connector is not connected to a key point the index will be -1. |
GetConnectorType | This method returns a member of the ConnectorTypeConstants constant set that specifies the type of the referenced Connector object. |
GetEndElement | This method returns the end element, end point and the key point index. If the connector is not connected to a key point the index will be -1. |
GetEndPoint | This method returns the coordinates of the referenced object's end point. |
GetEndTerminatorType | This method returns a member of the DimTermTypeTypeConstants constant set that specifies the type of the end terminator on the referenced Connector object. |
GetFlipState | This method returns the flip state of the connector. By default, the first segment of corner and step connectors is horizontal and when FlipState is TRUE, the first segment is vertical. For jump connectors, the start-to-end direction determines whether the arc is above or below the connector. When TRUE, only the arc is flipped. |
GetJumpRadius | This method returns the jump radius for the referenced Connector object. The radius is a factor of DimStyle.LineWidth, accessible through the Style property of the referenced Connector object. |
GetKeyPoint | Returns information about a specified key point. |
GetStartElement | This method returns the Start element, start point and the key point index. If the connector is not connected to a key point the index will be -1. |
GetStartPoint | This method returns the coordinates of the start point for the referenced object. |
GetStartTerminatorType | This method returns a member of the DimTermTypeTypeConstants constant set that specifies the type of the start terminator on the referenced Connector object. |
PromoteToCurrentVersion | Promotes connector to the latest version behavior, the same as if placing a new object. |
Range | Returns the high and low range values for the referenced object. |
Select | Selects the referenced object in the active window. |
SendBackward | Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it. |
SendToBack | Changes the display order of visible objects by moving the referenced object behind all overlapping objects. |
SetCenterElement | This method sets the center element on the connector. It is valid only for Jump Connector. Calling this method on Connector objects of other types will cause a run-time error. |
SetConnectorType | This method specifies the type of the referenced Connector object by passing a member of the ConnectorTypeConstants constant set. |
SetEndElement | This method sets the end element on the connector and connects to the end point if the index is not a key point index (-1). If the index is a valid key point index, the method ignores the point and connects to the index point. The method disconnect the previous end element, if it exists. If EndObj is NULL, the method disconnects the connector and makes it free space on the end side. |
SetEndPoint | |
SetEndTerminatorType | This method specifies the type of the end terminator on the referenced Connector object by passing a member of the DimTermTypeTypeConstants constant set. |
SetFlipState | This method sets the flip state of the connector. For corner and step connectors, pass TRUE to flip the connector from horizontal to vertical. For a jump connector, pass TRUE to flip the arc above the line. |
SetJumpRadius | This method sets the jump radius for the referenced Connector object. The radius is a factor of DimStyle.LineWidth, accessible through the Style property of the referenced Connector object. |
SetStartElement | This method sets the start element on the connector and connects to the start point if the index is not a key point index (-1). If the index is a valid key point index, the method ignores the point and connects to the index point. The method disconnect the previous start element, if it exists. If StartObj is NULL, the method disconnects the connector and makes it free space on the start side. |
SetStartPoint | This method relocates the starting point of the referenced object. |
SetStartTerminatorType | This method specifies the type of the start terminator on the referenced Connector object by passing a member of the DimTermTypeTypeConstants constant set. |