Solid Edge FrameworkSupport Type Library : DimensionStyle Object |
AboveGap | Sets and returns the gap between the dimension text and the dimension line when the text position is set to above. |
AllAroundMultiplier | |
AllowNegativeValueForCoordinate | Sets and returns the option to allow to set the negative values on coordinate dimensions |
AllowOriginValueChangeForCoordinate | Sets and returns the option to allow to change the coordinate origin dimension value |
AngularDecimalRoundOff | Sets and returns the angular round-off when angular units is set to degrees or radians and round off type is set to decimal. |
AngularDMSRoundOff | Sets and return the angular round off when angular units is set to Deg-Min-Sec. |
AngularFractionRoundOff | Sets and returns the angular round off when angular units is set to degrees or radians and round off type is set to fraction. |
AngularRoundOffType | Sets and returns the angular round off type (decimal or fraction) for the referenced dimension style object. |
AngularToleranceDecimalRoundOff | Sets and returns the angular tolerance decimal roundoff |
AngularToleranceDMSRoundOff | Sets and returns the angular tolerance Degree Minute Second roundoff |
AngularToleranceFractionRoundOff | Sets and returns the angular tolerance fractional roundoff |
AngularToleranceRoundOffType | Sets and returns the angular tolerance round off type |
AngularToleranceUnits | Sets and returns the angular tolerance units |
AngularUnits | Sets and returns the angular dimensioning unit separate from the working units of the file. |
ApplyBreakLineGap | |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
AutoCenterProjectionLine | Sets and returns the center projection line. |
AutoPhase | If True, specifies that the negative dash gaps for the referenced style object are automatically extended based on the size of the edge. |
AutoSuppressDiameter | Specifies whether or not to automatically suppress the diameter symbol when a circle is measured by a radial or circular diameter dimension. |
CalloutTextAspectRatio | Sets the callout text aspect ratio for the style. |
CenterLineType | Sets and returns the centerline type name for the referenced object. |
CenterMarkExtension | Specifies whether keypoint extensions are used for the center mark. |
CenterMarkSize | Sets and returns the size of the center mark for the referenced style object. |
ChamferUse45DegreeCharacter | Specifies chamfer 45 degree character use. |
CommonOrigin | Sets and returns the type of the terminator displayed at the common origin of a coordinate dimension group. |
ConnectorColor | |
ConnectorLineType | |
ConnectorWidth | |
CoordinateAutoJog | Determines if the referenced coordinate dimension is jogged automatically when the dimension value is less than the coordinate stack pitch. |
CoordinateStackPitch | Sets and returns the minimum coordinate dimension value after which the coordinate dimension will be jogged when the CoordAutoJog property is set to True. |
CoordinateTextOrientation | Sets and returns the text orientation of Coordinate Dimension |
CoordinateTextPosition | Sets and returns the position of the coordinate text in relation to the projection line. |
DatumFrameDashes | Sets and returns the datum frame dashes for the referenced DatumFrame object. |
DatumFrameLineTermThickness | Sets and returns the datum frame line terminator thickness. |
DatumFrameShape | Sets and returns the datum frame shape. |
DatumTargetTerminatorType | Sets and returns the datum target terminator type. |
DatumTerminatorGap | Sets and returns the datum terminator gap. |
DatumTerminatorType | Sets and returns the datum terminator type. |
Delimiter | Sets and returns the delimiter for the referenced object. |
Description | Returns a user-specified description of the referenced object. |
DimensionScale | Sets and returns the scale factor of the referenced object. |
DimensionScaleMode | Sets and returns the scale mode of the referenced object. |
DisplayCoordinateOriginText | Sets and returns the display of coordinate origin text. |
DisplayDegreeSymbolOnNumericTolerance | Display degree symbol on numeric angular tolerance values. |
DrivenColor | Sets and returns the color in which driven dimensions are displayed. |
DrivingColor | Sets and returns the color in which driving dimensions are displayed. |
DualDisplay | Turns on and off the dual display for the referenced object. |
DualModeVerticalGap | Sets and returns the vertical gap distance between Dimension Value text when the DualModeDisplay property is True. |
DualUnitJustification | Sets and returns the dual unit justification,Only applicable for dual unit position below primary |
DualUnitPosition | Sets and returns the dual unit position |
EnableAutoJogForCoordinate | Sets and returns the option to allow enable automatic jogging on coordinate dimensions |
ErrorColor | Sets and returns the color in which dimensions in error are displayed. |
Font | Sets and returns the name of the font. |
FontStyle | Sets and returns the style of the font for the text of the referenced object. |
FractionSeparator | |
FreeSpaceTerminatorType | Sets and returns the type of terminator for an annotation whose terminator end is placed on a free-space point. |
Height | Returns the height of the referenced object. |
HeightPMI | |
HoleCalloutCounterbore | This read-write String property sets and returns the hole callout counterbore settings for the referenced object. |
HoleCalloutCounterboreThreaded | This read-write String property sets and returns the hole callout counterbore threaded settings for the referenced object. |
HoleCalloutCountersink | This read-write String property sets and returns the hole callout countersink settings for the referenced object. |
HoleCalloutCountersinkThreaded | This read-write String property sets and returns the hole callout countersink threaded settings for the referenced object. |
HoleCalloutSimple | This read-write String property sets and returns the hole callout simple settings for the referenced object. |
HoleCalloutSimpleThreaded | This read-write String property sets and returns the hole callout simple threaded settings for the referenced object. |
HoleShaftToleranceSeparatorType | Sets and returns class fit hole/shaft Separator type. |
HorizontalBoxGap | Sets and returns the horizontal gap for the dimension text box. |
HorizontalToleranceGap | Sets and returns the horizontal tolerance gap between the dimension value and tolerance text. |
InhibitZeroToleranceDisplay | |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
LeaderLineLength | Sets and returns the default leader distance. |
LimitTextArrangement | Sets and returns the arrangement of the dimension text for a limit dimension. |
LineConnect | Specifies whether or not a line is drawn between the terminators of a dimension when text and terminators are to be outside of the measured value. |
LineSpacing | Sets and returns the amount of space between two lines in a paragraph for the referenced object. |
LineWidth | Sets and returns the line width (in paper space units) for the referenced object. |
LowerCaseMultiplicationSymbol | This read-write Boolean property specifies whether the referenced object uses the lowercase multiplication symbol (x) for chamfer dimensions. |
MatchPrimaryDelimiter | |
MaximumSubunits | Sets and returns the maximum number of subunits displayed by the associated dimension before truncating and adding to the unit. |
MaximumViewAngle | Sets and returns the maximum view angle after which the associated dimension will not be displayed in a 3-D environment. |
Name | Returns the name of the referenced object. |
NTSSymbol | Sets and returns the display characteristics of a not-to-scale dimension for the referenced object. |
OffsetLeaderType | Sets and returns the type of offset leader to be drawn. |
OriginTerminatorType | Sets and returns the terminator type for the origin terminator of the referenced object. |
OrigTerminatorSize | |
OverridePulledOutText | |
OverridePulledOutText2 | Override dimension text position and orientation when dimension dragged along the dimension line. |
Parent | Returns the parent object for the referenced object. |
PlacePrefixInsideBasicDimensionBox | Sets and returns the placement of prefix inside basic dimension box. |
PrefixSuffixGap | Sets and returns the gap between prefix/suffix string and the dimension value text. |
PrimaryDecimalRoundOff | Sets and returns the accuracy for the primary decimal value. |
PrimaryFractionRoundOff | Sets and returns the accuracy for the primary fraction value. |
PrimaryLeadingZeros | Specifies whether or not the primary leading zeros are on. |
PrimaryLinearToleranceDecimalRoundOff | Sets and returns the primary linear tolerance decimal roundoff |
PrimaryLinearToleranceFractionRoundOff | Sets and returns the primary linear tolerance fractional roundoff |
PrimaryLinearToleranceFractionSeparator | Sets and returns the primary linear tolerance fraction separator |
PrimaryLinearToleranceMaximumSubunits | Sets and returns the primary linear tolerance maximum subunits |
PrimaryLinearToleranceRoundOffType | Sets and returns the primary linear tolerance round off type |
PrimaryLinearToleranceSubunitsLabel | Sets and returns the primary linear tolerance subunit label |
PrimaryLinearToleranceUnitLabel | Sets and returns the primary linear tolerance unit label |
PrimaryLinearToleranceUnits | Sets and returns the primary linear tolerance units |
PrimarySubunitsLabel | Sets and returns the text string for the primary subunits label. |
PrimaryTrailingZeros | Specifies whether or not primary trailing zeros are on. |
PrimaryUnitLabel | Sets and returns the text string of the primary unit's label. |
PrimaryUnits | Sets and returns the dimensioning unit separate from the working units of the file. |
ProjectionAngle | Sets and returns the angle of the projection lines with respect to the dimension text. |
ProjectionBreakGap | This property creates an override style on the dimension and updates the break gap. |
ProjectionExtensionGap | Sets and returns the distance by which the projection lines are extended beyond the dimension line. |
ProjectionLineDisplay | Specifies the projection line direction. |
ProjectionOffsetGap | Sets and returns the gap between the object being measured and the projection line. |
ProjectionOffsetGapAlignment | Specifies whether or not the projection offset is aligned. |
ProjectionToleranceZonePosition | Sets and returns the projection tolerance position for the dimension. |
PulledOutText2Orientation | Sets and returns the text orientation of OverridePulledOutText2. |
PulledOutText2Position | Sets and returns the text orientation of OverridePulledOutText2. |
PulledOutTextOrientation | |
PulledOutTextPosition | |
Ratio | Sets and returns the text aspect ratio. |
RoundOffType | Sets and returns the round off type. |
RoundUp | Sets and returns round up type (round up all or round up odd) for the referenced dimension style object. |
SecondaryDecimalRoundOff | Sets and returns the accuracy for the secondary decimal value. |
SecondaryDelimiter | |
SecondaryFractionRoundOff | Sets and returns the accuracy for secondary fraction value. |
SecondaryLeadingZeros | Specifies whether or not secondary leading zeros are on. |
SecondaryLinearFractionSeparator | Sets and returns the secondary linear fraction separator |
SecondaryLinearRoundOffType | Sets and returns the secondary linear roundoff type. |
SecondaryLinearToleranceDecimalRoundOff | Sets and returns the secondary linear tolerance decimal roundoff |
SecondaryLinearToleranceFractionRoundOff | Sets and returns the secondary linear tolerance fractional roundoff |
SecondaryLinearToleranceFractionSeparator | Sets and returns the secondary linear tolerance fraction separator |
SecondaryLinearToleranceMaximumSubunits | Sets and returns the secondary linear tolerance maximum subunits |
SecondaryLinearToleranceRoundOffType | Sets and returns the secondary linear tolerance round off type |
SecondaryLinearToleranceSubunitsLabel | Sets and returns the secondary linear tolerance subunit label |
SecondaryLinearToleranceUnitLabel | Sets and returns the secondary linear tolerance unit label |
SecondaryLinearToleranceUnits | Sets and returns the secondary linear tolerance units |
SecondarySubunitsLabel | Sets and returns the text string for the secondary subunits label. |
SecondaryToleranceEquivalent | Specifies whether or not the secondary tolerance is equivalent. |
SecondaryTrailingZeros | Specifies whether or not the secondary trailing zeros are on. |
SecondaryUnitLabel | Sets and returns the text string for the secondary units label. |
SecondaryUnitRoundOff | Sets and returns the round off type for secondary units. |
SecondaryUnits | Sets and returns the secondary dimensioning unit. |
SecondaryUnitSeparator | Sets and returns the secondary unit separator. |
ShowOriginLineForCoordinate | Sets and returns the option to allow to display the coordinate origin dimension line |
SlotCalloutCounterbore | Sets and returns text for Counterbore slots. |
SlotCalloutSimple | Sets and returns text for Simple slots. |
SmartDepthHoleFinite | Sets and returns SmartDepth for finite holes. |
SmartDepthHoleThru | Sets and returns SmartDepth for through holes. |
SmartDepthSlotFinite | Sets and returns SmartDepth text for finite slots. |
SmartDepthSlotThru | Sets and returns SmartDepth text for through slots. |
SmartDepthThreadFinite | Sets and returns SmartDepth for finite threads. |
SmartDepthThreadThru | Sets and returns SmartDepth for through threads. |
StackPitch | Sets and returns the minimum distance track distance maintained between individual dimensions within a group. |
SymbolFont | Sets and returns the Symbol Font used by this style. |
SymbolGap | Sets and returns the gap between the dimension symbol and the dimension value text. |
SymbolPosition | Sets and returns the symbol position with respect to the dimension text value. |
TerminatorDisplay | Sets and returns the terminator display. |
TerminatorInsideLimit | Toggles the associated dimension to the outside of the projection when the dimension value is less than the terminator inside limit. |
TerminatorSize | Sets and returns the size of the terminator for the referenced DimensionStyle object. |
TerminatorType | Sets and returns the type of terminator for both origin and measure. |
TextAutoFillBackground | |
TextClearanceGap | Sets and returns the gap distance between the dimension text and the dimension line. |
TextOrientation | Sets and returns the orientation of the dimension text with respect to the dimension plane axis. |
TextPosition | Sets and returns the text position. |
TextWeight | Sets and returns the text line width. |
ThreeSidedSymbolOffsetGap | Sets and returns the offset gap value of Three Sided Weld Symbol. |
ToleranceHeightRatio | Sets and returns the tolerance height. |
ToleranceTextHorizontalAlignment | Sets and returns horizontal alignment for upper and lower tolerance. |
ToleranceTextVerticalAlignment | Sets and returns vertical alignment for tolerance text. |
ToleranceWeight | Sets and returns the tolerance text weight. |
UseTextSizeForCombinedTolValueDisplay | If True, specifies that the dimension text size will be used for the tolerance when upper and lower tolerance have the same absolute value but opposite signs. |
VerticalBoxGap | Sets and returns the vertical gap for the text box. |
VerticalLimitsGap | Sets and returns the vertical limits gap between the limit value texts. |
VerticalToleranceGap | Sets and returns the vertical tolerance gap between the dimension value and the tolerance text. |
ViewCaptionLocation | Sets and returns the caption location of the drawing view. |
ViewCPLCaptionLocation | Sets and returns the caption location of the cutting plane line display. |
ViewCuttingPlaneLineDisplay | Sets and returns the direction of the terminator. |
ViewLineArrowOffset | |
ViewLineType | Sets and returns the name of the view line type to be displayed for the referenced object. |
ViewLineWidth | Sets and returns the line width of the viewing and cutting plane lines. |
ViewPlaneLineDisplay | Sets and returns the number of terminator lines displayed. |
ViewSuffixAsPrefix | Sets and returns the suffix as prefix for drawing view caption. |
ViewTerminatorRatio | Sets and returns the size of the terminator on the viewing and cutting plane lines. |
ViewTextRatio | Sets and returns the size of caption text displayed on the drawing view. |
ViewThickLineLength | |
ViewThinTerminator | Sets and returns the thin/thick direction lines of cutting plane line or view plane lines. |
ViewVPLCaptionAtEnd | Sets and returns the caption location of the view plane. |
WeldSymbolLineWidth | Sets and returns the line width of Weld Symbol. This value is always in meters. |
ZeroInchesForFTIN | Display leading zero for inches when value includes fraction of inch for unit type Feet-Inch. |