Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objDimStyles As SolidEdgeFrameworkSupport.DimensionStyles
Dim objANSImmDimStyle As SolidEdgeFrameworkSupport.DimensionStyle
Dim objTempStyle As SolidEdgeFrameworkSupport.DimensionStyle
Dim lngCount As Long
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Get the DimensionsStyles collection object
Set objDimStyles = objDoc.DimensionStyles
'Get the number of default Styles available. This is required bcause the new style
'will be added at the end of the collection.
lngCount = objDimStyles.Count
'Add a New DimStyle
Set objANSImmDimStyle = objDimStyles.Add(Name:="DimStyle1", Parent:="ANSImm")
'Get another reference to the newly created DimStyle using the Item method.
Set objTempStyle = objDimStyles(lngCount + 1)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objDimStyles = Nothing
Set objANSImmDimStyle = Nothing
Set objTempStyle = Nothing
End Sub