Solid Edge FrameworkSupport Type Library
CoordinateAutoJog Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimensionStyle Object
: CoordinateAutoJog Property
Description
Determines if the referenced coordinate dimension is jogged automatically when the dimension value is less than the coordinate stack pitch.
Property type
Read-write property
Syntax
Visual Basic
Public Property CoordinateAutoJog As Boolean
See Also
DimensionStyle Object
|
DimensionStyle Members