Imports System.Runtime.InteropServices
Public Class SmartDepthSlotThru
Private Sub btnSmartDepthSlotThru_Click(sender As System.Object, e As System.EventArgs) Handles btnSmartDepthSlotThru.Click
Dim objApplication As SolidEdgeFramework.Application = Nothing
Dim objDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
Dim objDimStyles As SolidEdgeFrameworkSupport.DimensionStyles = Nothing
Dim objTempStyle As SolidEdgeFrameworkSupport.DimensionStyle = Nothing
Dim objType As Type = Nothing
Dim strThroughSlot As String
Try
' Create/get the application with specific settings
objApplication = Marshal.GetActiveObject("SolidEdge.Application")
If objApplication Is Nothing Then
' Get the type from the Solid Edge ProgID
objType = Type.GetTypeFromProgID("SolidEdge.Application")
' Start Solid Edge
objApplication = Activator.CreateInstance(objType)
' Make Solid Edge visible
objApplication.Visible = True
End If
objDraftDoc = objApplication.ActiveDocument
'Get the DimensionsStyles collection object
objDimStyles = objDraftDoc.DimensionStyles
'Get reference to first DimStyle.
objTempStyle = objDimStyles(0)
'Set the smart depth for Through slot
objTempStyle.SmartDepthSlotThru = "THRU"
'Get the smart depth for Through slot
strThroughSlot = objTempStyle.SmartDepthSlotThru
If strThroughSlot <> "THRU" Then
MsgBox("Error in SmartDepthSlotThru property for dimension style.")
End If
Catch ex As Exception
MsgBox(ex.ToString)
End Try
End Sub
End Class