Solid Edge FrameworkSupport Type Library
AddByCenter Method
The coordinates of the center point of the ellipse.
The coordinates of the center point of the ellipse.
The coordinates of the point that defines the end of the major axis for the ellipse.
The coordinates of the point that defines the end of the major axis for the ellipse.
Specifies the ratio of the length of the minor axis relative to the major axis.
A member of the Geom2dOrientationConstants constant set that specifies the direction (clockwise or counterclockwise) in which the ellipse is drawn from the major axis.
Description
Uses a center point to create a CenterMark, Ellipse2d, or EllipticalArc2d object.
Syntax
Visual Basic
Public Function AddByCenter( _
   ByVal xCenter As Double, _
   ByVal yCenter As Double, _
   ByVal xMajor As Double, _
   ByVal yMajor As Double, _
   ByVal Ratio As Double, _
   ByVal Orientation As Geom2dOrientationConstants _
) As Ellipse2d
Parameters
xCenter
The coordinates of the center point of the ellipse.
yCenter
The coordinates of the center point of the ellipse.
xMajor
The coordinates of the point that defines the end of the major axis for the ellipse.
yMajor
The coordinates of the point that defines the end of the major axis for the ellipse.
Ratio
Specifies the ratio of the length of the minor axis relative to the major axis.
Orientation
ValueDescription
igGeom2dOrientClockwiseObjects drawn Clockwise
igGeom2dOrientCounterClockwiseObjects drawn Counter Clockwise
A member of the Geom2dOrientationConstants constant set that specifies the direction (clockwise or counterclockwise) in which the ellipse is drawn from the major axis.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllipses As SolidEdgeFrameworkSupport.Ellipses2d
    Dim objEllipse As SolidEdgeFrameworkSupport.Ellipse2d
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an Ellipses collection object
    Set objEllipses = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).Ellipses2d
    'Create an Ellipse object
    Set objEllipse = objEllipses.AddByCenter(xCenter:=0, yCenter:=0, xMajor:=0.01, _
                                             yMajor:=0, Ratio:=0.5, Orientation:=igGeom2dOrientClockwise)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllipses = Nothing
    Set objEllipse = Nothing
End Sub
See Also

Ellipses2d Collection  | Ellipses2d Members