Solid Edge FrameworkSupport Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Application
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllipses As SolidEdgeFrameworkSupport.Ellipses2d
    Dim objApplicn As SolidEdgeFramework.Application
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an Ellipses collection object
    Set objEllipses = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).Ellipses2d
    ' Get the Application Property
    Set objApplicn = objEllipses.Application
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllipses = Nothing
    Set objApplicn = Nothing
End Sub
See Also

Ellipses2d Collection  | Ellipses2d Members