Solid Edge FrameworkSupport Type Library : FeatureControlFrameDataSet Object |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BoxAlignment | Sets and returns the status of the alignment of a feature control frame. Note: This is a multi-level feature control option. if it's set true value, all first and second box would align and text move to the center of box. |
CompositePrimaryAndSecondaryText | Sets and returns the composite status of primary and secondary text. |
CompositeSecondaryAndTertiaryText | Sets and returns the composite status of secondary and tertiary text. |
CompositeTertiaryAndQuaternaryText | Sets and returns the composite status of tertiary and quaternary text. |
FCFAllAround | Specifies whether or not an all around symbol is to be applied to the Leader of the referenced object. |
FCFAllOver | Specifies whether or not an all over symbol is to be applied to the Leader of the referenced object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
PrimaryFrame | Sets and returns the primary frame text. |
QuaternaryFrame | Sets and returns the quaternary frame text. |
SecondaryFrame | Sets and returns the secondary frame text for the referenced FeatureControlFrame object. |
TertiaryFrame | Sets and returns the tertiary frame text. |