AddVertex | Creates a vertex at the end of the object. |
BringForward | Changes the display order of the referenced object by moving it in front of the first object that obscures it. |
BringToFront | Changes the display order of the referenced object by moving it in front of all other overlapping objects. |
Copy | Places a copy of the referenced object on the clipboard. |
Cut | Moves the referenced object to the system clipboard. |
Delete | Deletes the referenced object. |
Duplicate | Copies the referenced object to a specified location, creating a new instance of the object with the same property values as the original. |
GetConnect | Returns the object to which the referenced Leader object connects. |
GetConnectPoint | Returns the location of the terminal connect point for the referenced Leader object. |
GetDisplayData | |
GetFreeSpacePoint | Returns the coordinates of the terminal connect point for a leader line that belongs to the active dimensioning object. |
GetKeyPoint | Returns information about a specified key point. |
GetTerminator | Returns the object to which the terminal end of a dimensioning or annotation object's leader connects. |
GetVertex | Returns the coordinates of the referenced object based on a specified index. |
GetVertices | Returns an array of vertex coordinates in a dimensioning object. |
InsertVertex | Adds a vertex at a specified index causing indices of following vertices to increment by one. |
Mirror | Copies the referenced object about an axis. |
Move | Moves the referenced object. |
PromoteToCurrentVersion | Promotes leader to the latest version behavior, the same as if placing a new object. |
Range | Returns the high and low range values for the referenced object. |
RemoveVertex | Removes a vertex at a specified index, causing indices of following vertices to decrement by one. |
Rotate | Rotates the referenced object about the point specified by the angle in radians. |
Scale | Scales the referenced object by a specified factor. |
Select | Selects the referenced object in the active window. |
SendBackward | Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it. |
SendToBack | Changes the display order of visible objects by moving the referenced object behind all overlapping objects. |
SetConnect | Specifies the object to which the referenced Leader object connects. |
SetConnectPoint | Sets the location of the terminal connect point for the referenced Leader object. |
SetFreeSpacePoint | Specifies the coordinates of the terminal connect point for a leader line belonging to the referenced dimensioning object. |
SetKeyPoint | Sets the position for a specified key point. |
SetTerminator | Specifies a new object and/or connect point for the terminal end of an annotatino object's leader. |
SetVertex | Sets the coordinates of an existing vertex of the referenced object. |
SetVertices | Creates vertices in a dimensioning object from an array of x-y coordinates. |