Specifies the object to which the terminal end of a dimensioning or annotation object's leader connects.
Coordinates of the leader's terminal connect point on the TerminatorObj.
Coordinates of the leader's terminal connect point on the TerminatorObj.
Coordinates of the leader's terminal connect point on the TerminatorObj.
Returns True if the leader was placed with respect to the TerminatorObj. Returns False if the leader was placed with respect to a key point on the TerminatorObj.
Description
Returns the object to which the terminal end of a dimensioning or annotation object's leader connects.
Syntax
Visual Basic
Public Sub GetTerminator( _
ByRef TerminatorObj As Object, _
ByRef x As Double, _
ByRef y As Double, _
ByRef z As Double, _
ByRef keyPoint As Boolean _
)
Parameters
TerminatorObj
Specifies the object to which the terminal end of a dimensioning or annotation object's leader connects.
x
Coordinates of the leader's terminal connect point on the TerminatorObj.
y
Coordinates of the leader's terminal connect point on the TerminatorObj.
z
Coordinates of the leader's terminal connect point on the TerminatorObj.
keyPoint
Returns True if the leader was placed with respect to the TerminatorObj. Returns False if the leader was placed with respect to a key point on the TerminatorObj.
Remarks
This method also returns the coordinates of the leader's terminal connect point and a Boolean value to indicate whether the leader was placed with respect to the object or with respect to a key point on that object.