Solid Edge FrameworkSupport Type Library
PMI Object
Members 
Description
Object Model
PMI ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows Collection
Example
Imports System.Runtime.InteropServices
Public Class CreatePMIDimensions

    Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim ObjDoc As SolidEdgeFramework.SolidEdgeDocument = Nothing
        Dim objPartDoc As SolidEdgePart.PartDocument = Nothing
        Dim objdims As SolidEdgeFrameworkSupport.Dimensions = Nothing
        Dim objDim As SolidEdgeFrameworkSupport.Dimension = Nothing
        Dim objOrigDim As SolidEdgeFrameworkSupport.Dimension = Nothing
        Dim objPMI As SolidEdgeFrameworkSupport.PMI = Nothing
        Dim objEdges As SolidEdgeGeometry.Edges = Nothing
        Dim objLinearEdge1 As SolidEdgeGeometry.Edge = Nothing
        Dim objLinearEdge2 As SolidEdgeGeometry.Edge = Nothing
        Dim objDimPlane As SolidEdgePart.RefPlane = Nothing
        Dim objDimInitData As SolidEdgeFrameworkSupport.DimInitData = Nothing

        Dim dblStartPoint1(0) As Double
        Dim dblEndPoint1(0) As Double
        Dim dblStartPoint2(0) As Double
        Dim dblEndPoint2(0) As Double
        Dim dblStartPoint3(0) As Double
        Dim dblEndPoint3(0) As Double
    
        Try
            'Get the application with specific settings
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            'Need a Part file with a block in it.
            objPartDoc = objApplication.ActiveDocument
            'Get the PMI object from the document
            Call objPartDoc.PMI_ByModelState(PMIObj:=objPMI)

            'Get the dimensions collection from the PMI object
            objdims = objPMI.Dimensions

            objEdges = objPartDoc.Models.Item(1).ExtrudedProtrusions.Item(1).Edges(SolidEdgeGeometry.FeatureTopologyQueryTypeConstants.igQueryAll)

            If Not objEdges Is Nothing Then
                objLinearEdge1 = objEdges.Item(1)
                objLinearEdge2 = objEdges.Item(2)
            End If

            objDimPlane = objPartDoc.RefPlanes.Item(2)

            objDimInitData = objdims.DimInitData

            'linear distance between
            Call objDimInitData.ClearParents()
            Call objDimInitData.SetType(SolidEdgeFrameworkSupport.DimTypeConstants.igDimTypeLinear)
            Call objDimInitData.SetAxisMode(SolidEdgeFrameworkSupport.DimAxisModeConstants.igDimAxisModeDefault)
            Call objDimInitData.SetPlane(objDimPlane)
            Call objDimInitData.SetNumberOfParents(2)
            Call objLinearEdge1.GetEndPoints(StartPoint:=dblStartPoint1, EndPoint:=dblEndPoint1)
            Call objLinearEdge2.GetEndPoints(StartPoint:=dblStartPoint2, EndPoint:=dblEndPoint2)
            Call objDimInitData.SetParentByIndex(0, objLinearEdge1, True, False, False, False, dblStartPoint1(0), dblStartPoint1(1), dblStartPoint1(2))
            Call objDimInitData.SetParentByIndex(1, objLinearEdge2, True, False, False, False, dblStartPoint2(0), dblStartPoint2(1), dblStartPoint2(2))
            objDim = objdims.AddDimension(DimInitData:=objDimInitData)

        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try

    End Sub

End Class
See Also

PMI Members  | Solid Edge ST2 - What's New  | Solid Edge ST MP1 - What's New  | Solid Edge V20 SP10 - What's New