Solid Edge FrameworkSupport Type Library
SymbolicPMI Object
Members 
Description
Specifies all unique GOST weld types necessary in the fabrication of the weldment.
Object Model
SymbolicPMI ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows Collection
Example
Imports System.Runtime.InteropServices
Public Class Form1

    Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click
        Dim objApp As SolidEdgeFramework.Application = Nothing
        Dim objDoc As SolidEdgePart.PartDocument = Nothing
        Dim objsym As SolidEdgeFrameworkSupport.SymbolicPMI = Nothing
        Dim objPMIGroup As SolidEdgeFrameworkSupport.SymbolicPMIGroup = Nothing
        Dim objPMI As SolidEdgeFrameworkSupport.PMI = Nothing
        Dim i As Integer

        Try
            ' Create/get the application with specific settings
            objApp = Marshal.GetActiveObject("SolidEdge.Application")

            ' Get the active JT document containing symbolic PMI group.
            objDoc = objApp.ActiveDocument
            ' Get PMI
            objDoc.PMI_ByModelState(PMIObj:=objPMI)
            'Get symbolic PMI Group
            objPMIGroup = objPMI.SymbolicPMIGroup
 
            i = objPMI.SymbolicPMIGroup.count()
            objsym = objPMIGroup.Item(1)
            objsym.Delete()

        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try
    End Sub
End Class
See Also

SymbolicPMI Members