BottomNote1 | Sets and returns the Bottom Note 1 text for the referenced object. |
BottomNote2 | Sets and returns the Bottom Note 2 text for the referenced object. |
BottomNote3 | Sets and returns the Bottom Note 3 text for the referenced object. |
BottomNoteZ | Sets and returns the Bottom Note Z text for the referenced object. |
BottomTreatmentType | Sets and returns the treatment display style to use for the bottom treatment portion of the referenced object. |
BottomType | Sets and returns the bottom type for the referenced object. |
BottomWeldModifier | Sets and returns the bottom weld modifier for the referenced object. |
DashLine | Sets and returns the relative position of the dash lines for the referenced weld symbol object. |
OffsetTopBottom | Specifies whether the top and bottom weld types are offset or aligned. |
Symmetrical | Specifies whether or not the referenced object is symmetrical. |
Tail | Specifies whether the less than symbol appears at the end of the breaklline. |
TailNote | Sets and returns the tail note text. |
TopNote1 | Sets and returns the Top Note 1 text. |
TopNote2 | Sets and returns the Top Note 2 text. |
TopNote3 | Sets and returns the Top Note 3 text. |
TopNoteZ | Sets and returns the Top Note Z text. |
TopTreatmentType | Sets and returns the display style to use for the top treatment portion of the referenced object. |
TopType | Sets and returns the top type for the referenced object. |
TopWeldModifier | Sets and returns the top weld modifier for the referenced object. |
WeldAllAround | Specifies whether or not the 'weld all around' display style is included in the referenced object. |
WeldInField | Specifies whether or not the 'weld in field' display style is included in the referenced object. |
ZSymbol | Specifies whether or not the Z weld symbol modifier is included in the referenced object. |