Solid Edge Framework Type Library
BeforeCommandRun Event
The ID of the command for which the event is triggered.
Description
Occurs before a specified command is run.
Syntax
Visual Basic
Public Event BeforeCommandRun( _
   ByVal theCommandID As Long _
)
Parameters
theCommandID
The ID of the command for which the event is triggered.
See Also

ApplicationEvents Object  | ApplicationEvents Members