Active | Sets and returns the name of the active style object. |
Color | Sets and returns the color in which the active object is drawn. |
Description | Returns a user-specified description of the referenced object. |
FillBackground | Sets and returns the background color of the referenced object. |
FillColor | Sets and returns the color with which to fill the background of an object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
PatternName | Sets and returns the name of the active pattern. |
PatternType | Sets and returns the type of pattern to apply to the referenced FillStyle object. |
Rotation | For OLE objects, specifies the angle at which the object is rotated along its major axis. For hatch lines, sets and returns the rotation angle used to display hatch lines. |
Spacing | Sets and returns the distance between the primary hatch lines in a hatch pattern. |
Units | Sets and returns the units in which the line width is defined. |