Solid Edge Framework Type Library
HatchPatternStyle Object
Members 
Description
A vector pattern that is used to fill a closed boundary.
Remarks
The HatchPatternStyle object can contain multiple vector line styles oriented at any offset, angle, or spacing. The hatch pattern is constructed from one or more linear elements. These elements can be customized through the object's methods to use a specified line style, width, color, and point of origin. The distance at which the elements repeat in the fill area can also be customized.
See Also

HatchPatternStyle Members