Solid Edge Framework Type Library
ISEAddIn Object
Members
Collapse All
Expand All
Solid Edge Framework Type Library
: ISEAddIn Object
Description
A control that represents a command added to Solid Edge through the AddIn interface.
Object Model
Remarks
Addins written for V20 or later, it is preferred to implement the
ISEAddInEx
interface rather than the ISEAddIn interface.
See Also
ISEAddIn Members