Returns an array containing full paths to each Geometric Dirty file (including the top level document if it is Persist dirty.) The entries are listed in bottom-up order, which is the order in which they will saved when calling SaveChangedFiles().
Description
This method returns a list of dirty documents in the current tree scope.
Syntax
Visual Basic
Public Sub GetFilesToSave( _
ByRef FilesToSave() As String, _
Optional ByVal FutureUse As Variant _
)
Parameters
FilesToSave
Returns an array containing full paths to each Geometric Dirty file (including the top level document if it is Persist dirty.) The entries are listed in bottom-up order, which is the order in which they will saved when calling SaveChangedFiles().
FutureUse
Remarks
It is not necessary to call this method before calling SaveChangedFiles().