Solid Edge Framework Type Library > SheetMetalSensors Collection : AddVariableSensor Method |
Visual Basic |
---|
Public Function AddVariableSensor( _ ByVal variable As Object, _ ByVal Name As String, _ ByVal Description As String, _ ByVal LowerRange As Double, _ ByVal UpperRange As Double, _ ByVal MinimumThreshold As Double, _ ByVal MaximumThreshold As Double, _ ByVal Operator As SensorOperatorConstants, _ ByVal DisplayType As SensorDisplayTypeConstants, _ ByVal UpdateMechanism As SensorUpdateMechanismConstants _ ) As Object |
Value | Description |
---|---|
seSensorOperatorBetween | Sensor operator - between |
seSensorOperatorEqualTo | Sensor operator - equal to |
seSensorOperatorGreaterThan | Sensor operator - greater than |
seSensorOperatorInvalid | Invalid sensor operator |
seSensorOperatorLessThan | Sensor operator - less than |
seSensorOperatorNotBetween | Sensor operator - not between |
seSensorOperatorNotEqualTo | Sensor operator - not equal to |
Value | Description |
---|---|
seSensorDisplayTypeHorizontalRange | Sensor display - horizontal range |
seSensorDisplayTypeInvalid | Invalid sensor display |
seSensorDisplayTypeTrueFalse | Sensor display - true/false |
Value | Description |
---|---|
seSensorUpdateMechanismAutomatic | Automatic sensor update |
seSensorUpdateMechanismInvalid | Invalid sensor update mechanism |
seSensorUpdateMechanismManual | Manual sensor update |