Solid Edge Framework Type Library
SolidEdgeTCE Object
Members 
Description
Solid Edge Teamcenter Automation object.
Example
Imports System.Runtime.InteropServices
Public Class Form1

    Private Sub Button1_Click(sender As System.Object, e As System.EventArgs) Handles Button1.Click
        
        Dim objApp As SolidEdgeFramework.Application = Nothing
        Dim objSEEC As SolidEdgeFramework.SolidEdgeTCE = Nothing
        Dim objAsm As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim objOccurrences As SolidEdgeAssembly.Occurrences = Nothing
        Dim objOccurrence As SolidEdgeAssembly.Occurrence = Nothing
        Dim objDocuments As SolidEdgeFramework.Documents = Nothing
        Dim UserName As String
        Dim Password As String
        Dim Group As String
        Dim Role As String
        Dim URL As String

        Dim varInputList(1) As Object
        Dim FileItemID As String
        Dim FileItemRevID As String
        Dim FileDataSetName As String
        Dim FileRevisionRule As String
        Dim FolderName As String
        Dim temp(0, 0) As Object
        Dim CachePath As String = ""
        Dim filename As String
        Dim listoffiles As Object = Nothing

        Try
            'Get Active session of Solid Edge 
            objApp = Marshal.GetActiveObject("SolidEdge.Application")

            ' Teamcenter Mode
            objSEEC = objApp.SolidEdgeTCE
            ' Get default cache path
            objSEEC.GetPDMCachePath(CachePath)
            'GetActive Document
            objAsm = objApp.ActiveDocument
            'Specify Server Credentials
            UserName = "abc"
            Password = "abc"
            Group = ""
            Role = ""
            URL = "http://servername:port/tc"

            Call objSEEC.ValidateLogin(UserName, Password, Group, Role, URL)

            objDocuments = objApp.Documents
            'Open Assembly
            'objAsm = objDocuments.Open(CachePath + "\" + "025016.asm")
            'Details of the Part to be added in Assembly
            FileItemID = "025015"
            FileItemRevID = "A"
            FileDataSetName = "025015.par"
            FileRevisionRule = ""
            FolderName = ""


            'temp is a 2 dimensional array which is not optional
            'Download the file to cache
            objSEEC.DownladDocumentsFromServerWithOptions(FileItemID, FileItemRevID, FileDataSetName, SolidEdgeConstants.RevisionRuleType.LatestRevision, "", True, False, SolidEdgeConstants.TCDownloadOptions.COImplicit, temp)
            'Get Name of the file downloaded
            objSEEC.GetListOfIndirectFilesForGivenFile(FileItemID, FileItemRevID, FileDataSetName, "latest working", "", listoffiles)
            'objSEEC.GetMappedPropertiesForGivenFile(FileItemID, FileItemRevID, FileDataSetName, listoffiles)
            'Cast the object to get filename
            filename = DirectCast(DirectCast(listoffiles, Object())(0), String)
            objOccurrences = objAsm.Occurrences
            'Add the part to assembly file
            objOccurrences.AddByFilename(CachePath + "\" + filename)

        Catch ex As Exception
            MsgBox(ex.ToString)
            Clipboard.SetText(ex.ToString)
        End Try
    End Sub
End Class
See Also

SolidEdgeTCE Members  | Solid Edge V19 - What's New