Solid Edge Framework Type Library
Add Method
Specifies the name of the Variable object.
Specifies the formula used to derive a value for the Variable object.
Specifies the unit type of the Variable object. Valid values are members of the UnitTypeConstants constant set.
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Function Add( _
   ByVal pName As String, _
   ByVal pFormula As String, _
   Optional ByVal UnitsType As Variant _
) As Object
Parameters
pName
Specifies the name of the Variable object.
pFormula
Specifies the formula used to derive a value for the Variable object.
UnitsType
Specifies the unit type of the Variable object. Valid values are members of the UnitTypeConstants constant set.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objVariables As SolidEdgeframework.Variables
    Dim objVariable As SolidEdgeframework.variable
    Dim objVar1 As SolidEdgeframework.variable
    Dim objVar2 As SolidEdgeframework.variable
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get Variables Collection
    Set objVariables = objDoc.Variables
    'Create a variable with Add method
    Set objVariable = objVariables.Add(pName:="Variable1", pFormula:="100.0")
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objVariables = Nothing
    Set objVariable = Nothing
    Set objVar1 = Nothing
    Set objVar2 = Nothing
End Sub
See Also

Variables Collection  | Variables Members