Solid Edge Framework Type Library
Edit Method
Specifies the name of the Variable object whose formula is to be edited.
Specifies the new formula.
Description
Edits the formula for the referenced Variable object.
Syntax
Visual Basic
Public Sub Edit( _
   ByVal pName As String, _
   ByVal pFormula As String _
) 
Parameters
pName
Specifies the name of the Variable object whose formula is to be edited.
pFormula
Specifies the new formula.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objVariables As SolidEdgeframework.Variables
    Dim objVariable As SolidEdgeframework.variable
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get Variables Collection
    Set objVariables = objDoc.Variables
    'Create a variable with Add method
    Set objVariable = objVariables.Add(pName:="Variable1", pFormula:="100.0")
    'Modify the formula of the varialbe with Edit method
    objVariables.Edit pName:="Variable1", pFormula:="Sin(30)"
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objVariables = Nothing
    Set objVariable = Nothing
End Sub
See Also

Variables Collection  | Variables Members