Solid Edge Framework Type Library
GetName Method
Specifies the Variable object for which to retrieve the name.
Description
Returns the name of the referenced Variable object.
Syntax
Visual Basic
Public Function GetName( _
   ByVal pVariable As Object _
) As String
Parameters
pVariable
Specifies the Variable object for which to retrieve the name.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objVariables As SolidEdgeframework.Variables
    Dim objVariable As SolidEdgeframework.variable
    Dim strName As String
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get Variables Collection
    Set objVariables = objDoc.Variables
    'Create a variable with Add method
    Set objVariable = objVariables.Add(pName:="Variable1", pFormula:="100.0")
    'Get the Name of objVariable
    strName = objVariables.GetName(pvariable:=objVariable)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objVariables = Nothing
    Set objVariable = Nothing
End Sub
See Also

Variables Collection  | Variables Members