AddLight | Adds a light to the referenced ViewStyle object. |
BeginPropertyBuffer | |
Delete | Deletes the referenced object. |
DeleteLight | Deletes a light from the referenced ViewStyle object. |
FlushPropertyBuffer | Flushes the property buffer for the referenced FaceStyle or ViewStyle object. |
GetAnalysisParameters | Returns the analysis parameters of the referenced ViewStyle object. |
GetGradientBackground | |
GetGradientColor | |
GetLight | Returns the parameters of a specified light for the referenced ViewStyle object. |
GetLightColor | Returns the color of a specified light for the referenced ViewStyle object. |
GetLightIntensity | Returns the intensity of a specified light for the referenced ViewStyle object. |
GetLightPhi | Returns the angle of the rotation in a spherical coordinate system of a specified light relative to the target for the referenced ViewStyle object. |
GetLightTheta | Returns the angle of the sweep in a spherical coordinate system of a specified light relative to the target for the referenced ViewStyle object. |
GetSkyboxOrientation | Returns the orientation of the skybox used in the referenced ViewStyle object. |
GetSkyboxSideFilename | Returns the file name of the image used on one side of the skybox in the referenced ViewStyle object. |
SetAnalysisParameters | Sets the analysis parameters of the referenced ViewStyle object. |
SetGradientBackground | |
SetGradientColor | |
SetLight | Sets the parameters of a specified light for the referenced ViewStyle object. |
SetLightColor | Sets the color of a specified light for the referenced ViewStyle object. |
SetLightIntensity | Sets the intensity of a specified light for the referenced ViewStyle object. |
SetLightPhi | Sets the angle of the rotation in a spherical coordinate system of a specified light relative to the target for the referenced ViewStyle object. |
SetLightTheta | Sets the angle of the sweep in a spherical coordinate system of a specified light relative to the target for the referenced ViewStyle object. |
SetSkyboxOrientation | Sets the orientation of the skybox used in the referenced ViewStyle object. |
SetSkyboxSideFilename | Sets the file name of the image used on one side of the skybox in the referenced ViewStyle object. |
SetSkyboxSkyFile | Sets the name of the sky file used to define the skybox in the referenced ViewStyle object. |
SkyboxClear | Clears the image from one side of the skybox in the referenced ViewStyle object. |
SkyboxClearAll | Clears the images from all sides of the skybox in the referenced ViewStyle object. |