AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DisplayName | This read-only String property returns the display name for the referenced object. |
Expose | This read-write Long property sets and returns whether the referenced object is exposed as a custom property. When set to 1, the object is exposed; when set to 0, the object is not exposed. |
ExposeName | This read-write String property sets and returns the name of the referenced object when the object is exposed as a custom property. |
Formula | Sets and returns the formula of the referenced Variable object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
IsSuppressVariable | |
Name | Returns the name of the referenced object. |
Properties | Sets and returns the variable properties. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |
UnitsType | Returns the unit type of the referenced Variable object. |
Value | Returns the name of the application, the value of a dimension, the value of a custom property, or the value of a variable. |
VariableTableName | Returns the name of the referenced object. |