Solid Edge Geometry Type Library
BSplineSurface Object
Members 
Description
Describes the B-Spline surface of the faces of a solid.
Remarks
Faces of a solid can be extracted using the Faces and FacesByRay properties on the model, feature, and topology objects, where each face is returned as a topology object collection. The geometric information is obtained from the face by using the Geometry property of the associated topology object. The U and V directions are directly implied by the surface definition.
See Also

BSplineSurface Members