Solid Edge Geometry Type Library
Edge Object
Members 
Description
Represents the elemental piece of the 3-D geometry information for the boundaries of a Face.
Remarks
It can be shared by at most two Faces, implying that the Faces are stitched at the current Edge. Though there is an independent flow direction of a given Edge, it has meaning only when viewed through the sense information stored in the associated EdgeUse object. It is then possible to view it as flowing in accordance with the Loop.
See Also

Edge Members