Solid Edge Geometry Type Library
EdgeUse Object
Members
Collapse All
Expand All
Solid Edge Geometry Type Library
: EdgeUse Object
Description
Represents the use of a given Edge in a loop.
Remarks
The Edge can belong to more than one Loop. The EdgeUse object holds the information about the direction in which the Edge must flow to be consistent with the Loop. It also holds the adjacent Face information through its Partner property.
See Also
EdgeUse Members