Solid Edge Geometry Type Library : Face Object |
GetBendCenterLineAttributes | Returns the bend center line attributes, if any. |
GetBendCenterLineAttributesEx | Returns the bend center line attributes, if any. |
GetCurvatures | Computes the minimum and maximum curvatures of the surface at a given parametric point on the surface. |
GetDerivatives | Evaluates the derivatives of the referenced curve at the points given by an array of parameters on the curve. |
GetExactRange | Returns the exact range for the referenced object. |
GetFacetData | Returns the number of facets and the number of points on the facets for the referenced object. If Tolerance <= 0, then data is returned from the geometry cache, and not from Parasolid. |
GetNormal | Given an array of parametric points, returns normal unit vectors. |
GetParamAnomaly | Returns information that indicates any parametric spaces with periodicity that might exist on a referenced edge. |
GetParamAtPoint | Computes the parameter on the curve that corresponds to a given array of world space points in the coordinate system lying near the curve. |
GetParamOnFace | Determines whether specified parameter lies within the trimmed region defined by the boundaries on the surface. |
GetParamRange | Returns the parametric extents in the U, V space of the surface within which all its boundaries lie. |
GetPointAtParam | Computes the corresponding model space points in the local coordinate system, given an array of parameters on the curve. |
GetRange | Returns the minimum and maximum points of the range for the referenced object. |
GetReferenceKey | Returns a reference key for the referenced object. |
GetTangents | Computes the two unit-vector tangents, given an array of parametric points on the surface. |
Application | Returns the active application object. |
Area | Returns the area of the referenced object. |
Body | Returns the Body object for the referenced object. |
Continuity | Returns the continuity of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
FacetCount | Returns the number of facets on the referenced object. |
Geometry | Returns a 3-D geometry object whose properties and methods can extend to the topology collection. |
GeometryForm | Specifies the geometry form of the referenced object. |
ID | Returns the Parasolid ID of the Face. |
IsParamReversed | Returns a Boolean value to specify whether or not the inherent direction of the referenced object is opposed to the flow dicated by the parameterization of the underlying geometry. |
Loops | Returns the Loops object collection for the referenced object. |
Parent | Returns the parent object for the referenced object. |
Shell | Returns the Shell object for the referenced object. |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
Tag | Returns the Tag of the Face. |
Type | Returns a member of the GNTTypePropertyConstants set to indicate the type of the referenced object. |
UpdatesCounter | Returns the number of times the referenced object has been modified. |
Vertices | Returns the Vertices object collection. |