Solid Edge Geometry Type Library
Plane Object
Members 
Description
Represents the plane surface geometry to provide access to information about the faces of a solid.
Remarks
Faces of a solid can be extracted using the Faces and FacesByRay properties on the Model and feature objects where each face is returned as a topological object. The geometric information is obtained from the face by using the Geometry property of the associated topological object. The U and V directions are not explicitly accessible through this object.
See Also

Plane Members