Solid Edge Geometry Type Library
Torus Object
Members 
Description
Represents the torus surface geometry to provide access to information about the faces of a solid.
Remarks
Faces of a solid can be extracted using the Faces and FacesByRay properties on the Model and feature objects where each face is returned as a topological object. The geometric information is obtained from the face by using the Geometry property of the topological object.
See Also

Torus Members