Solid Edge Part Type Library
Bead Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method GetDimensionsReturns the Dimensions collection object for the referenced object.
Public Method GetProfilesReturns the profiles associated with the referenced feature object.
Public Method GetStatusExReturns the status of the specified object.
Public Method GetStyleReturns the feature style.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method ReorderInserts the referenced object in front of or behind another feature.
Public Method RollToFeatureRolls the referenced Model object back to a specified feature.
Public Method SetProfilesSets the profiles associated with the referenced feature object.
Public Method SetStyleSets the feature style.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property CrossSectionTypeThe shape of the cross section of a Bead. Circular, U shaped, or V shaped.
Public Property DieRadiusThe radius of the rounding applied to the die side of the feature.
Public Property DisplayNameThis read-only String property returns the display name for the referenced object.
Public Property EdgebarNameThis read-only property returns the Edgebar name of the referenced object.
Public Property EdgesReturns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces.
Public Property EndConditionThe end treatment applied to an open profile Bead. Formed, Lanced, or Punched
Public Property EndPunchWidthThe width of a punched end Bead.
Public Property FacesReturns a collection of faces of a specified type that belong to a model, a feature, or a topology object.
Public Property FacesByRayReturns a collection of faces that are intersected by a specified vector.
Public Property FormRadiusThe radius of a Circular or V shaped Bead.
Public Property HeightThe height of the Bead.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property ModelingModeType
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property ProfileSets and returns the Profile object used to construct the referenced feature object.
Public Property PunchRadiusThe radius of the rounding applied to the punch side of the feature.
Public Property RoundingOptionWhether or not to apply rounding to the Bead feature.
Public Property ShowDimensionsControls the display of dimensions for the feature object.
Public Property SideThe side of offset of the Bead with respect to the Plate on which it resides.
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SuppressVariableReturns the suppress variable object.
Public Property SystemNameThis read-only String property returns the system name for the referenced object.
Public Property TaperAngleThe angle of the sides of a U shaped or V shaped Bead.
Public Property TypeSpecifies the type of the object being referenced.
Public Property VisibleSpecifies whether or not the referenced object is displayed to the screen.
Public Property WidthThe width of a U shaped Bead.
See Also

Bead Object