Solid Edge Part Type Library
BendAngle Property
Collapse All
Expand All
Solid Edge Part Type Library
>
Bend Object
: BendAngle Property
Description
Sets and returns the angle of the bend with respect to the stationary portion of the face to which the bend is added.
Property type
Read-write property
Syntax
Visual Basic
Public Property BendAngle As Double
See Also
Bend Object
|
Bend Members